The distances of the buss bars from the sides of the N8900 series are 197.5 mm and 247.5 mm respectively.
The instrument dimensions are in the manual. See http://literature.cdn.keysight.com/litweb/pdf/N8900-90901.pdf#page=19.
Note that Keysight has special rack supports (model number N8958A) for mounting these power supplies in Keysight racks. This is because these power supplies are wider than “standard” power supplies and will interfere with the standard rack supports.
Applies to: N8920A, N8921A, N8923A, N8924A, N8925A, N8926A, N8928A, N8929A, N8930A, N8931A, N8932A, N8934A, N8935A, N8937A, N8937APV, N8940A, N8941A, N8943A, N8944A, N8945A, N8946A, N8948A, N8949A, N8950A, N8951A, N8952A, N8954A, N8955A, N8957A, N8957APV
Visit our Power Products Forum for additional topics and discussions. Read technical postings on our Power Blog – Watt’s Up? |